Start an application automatically on a PanelView Plus CE terminal using parameters
On a
PanelView Plus CE
terminal, you can set up FactoryTalk View ME Station
to start and run an application automatically whenever the terminal starts by setting up the startup options or using parameters.To start an application automatically when a
PanelView Plus CE
terminal starts- Copy the path to the MERuntime.exe file (FactoryTalk View ME Station) to the WindowsStartupfolder.The default folders of the path to the MERuntime.exe file is\Storage Card\Windows\Desktop.The WindowsStartupfolder is\Storage Card\Windows\Startup.
- In theStartupfolder, right-clickFactoryTalk View ME Stationand selectProperties.
- On thetab, in theShortcutbox, after the existing text, type a space, the path to the .mer file, and one or more parameters.TargetFor example, to start FactoryTalk View ME Station and open an application file in a default folder, calledMalthouse, type:"\Storage Card\Rockwell Software\RSViewME\Runtime\Malthouse.mer" /r /d /o
- ClickOK.
In the future, whenever the
PanelView Plus CE
terminal starts, FactoryTalk View ME
Station will start automatically, delete the applications log files, overwrite the terminal's communications file, and run the application.If you do not want to delete the log files, omit the
/d
parameter.If you do not want to overwrite the communications file, omit the
/o
parameter.To give the user the choice of overwriting the communications file, use the
/a
parameter instead of the /o
parameter.
TIP:
If your application uses a shared network folder to store data log files, you will have to log onto a network when the application starts. To run the application automatically, you must store the network logon data in the terminal's permanent storage.
Provide Feedback