Message tab of the Alarm Setup editor

On the
Messages
tab of the
Alarm Setup
editor, specify trigger values and messages for the triggers you defined on the Triggers tab of the Alarm Setup editor.
TIP:
The
Delete Row(s)
menu item on the
Edit
menu does not delete multiple selected rows in certain spreadsheet editors. If you select multiple rows in the
Information Messages
,
Local Messages
,
Macros
,
and Alarm Setup (Messages tab)
editors, and then select
Delete Row(s)
from the
Edit
menu, only one row will be deleted.
To delete multiple rows, right-click in the editor and select
Delete Row(s)
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal