Triggers tab of the Alarm Setup editor

On the
Triggers
tab of the Alarm Setup editor, specify the tags or expressions to monitor for alarm conditions.
For each trigger, specify the type of data the trigger uses. You can also set up handshaking and acknowledgment features for the trigger, if required, and specify a message connection to which the message text can be sent.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal