Remove an alarm trigger

You may need to remove an alarm trigger.
To remove an alarm trigger
  1. On the Triggers tab of the Alarm Setup editor, from the
    Select trigger
    list, select the trigger and click
    Remove
    .
  2. Click
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal