Edit an alarm trigger
You may need to edit an alarm trigger.
To edit an alarm trigger
- On the Triggers tab of the Alarm Setup editor, in theSelect triggerlist, click the trigger to edit.
- To change the tag or expression assigned to the trigger, clickEditto make changes in the Trigger dialog box.
- To change other properties for the trigger, such asTrigger Type, make changes in theTrigger settingsarea of theAlarm Setupeditor.IMPORTANT:An alarm’sTriggerandRemote Acksettings should not be configured to use the same tag. Doing so may cause unpredictable alarm acknowledgment behaviors.
Provide Feedback