Delete an alarm message
Use the Messages tab of the Alarm Setup editor to delete an alarm message.
To delete an alarm message
- On theMessagestab of theAlarm Setupeditor, select a cell in the message's row and pressDelete, or right-click the cell and selectDelete Row(s).TIP:To delete multiple alarm messages, pressShiftorCtrlto select multiple cells in a column, right-click the selected cells and selectDelete Row(s).
Provide Feedback