Create an alarm message
Use the Message tab of the Alarm Setup editor to create an alarm message.
To create an alarm message
- On theMessagestab of theAlarm Setupeditor, in theTriggercolumn, select the trigger for which to create an alarm message.
- Specify the properties for the trigger.TIP:If the application is not aPanelView Plus 7 Standardapplication that has 500 alarm messages, or aPanelView Plus 6 Compactapplication that has 200 alarm messages, specifying the properties (exceptBackgroundandForeground) for the trigger in the last row will add an unassigned trigger.
- Repeat steps 1 and 2 to set up additional messages.
Provide Feedback