Import and conversion of an application

You can import the following application files to
FactoryTalk View Studio
and convert them to the current version
FactoryTalk View ME
application files using Machine Edition Import Wizard:
  • RSView®
    Machine Edition application (.med)
  • FactoryTalk View ME
    application (.med)
When importing an application:
  • If the application contains any direct driver nodes, the Import Wizard will create an RSLinx topic for each direct driver node it finds. All topics are then converted to device shortcuts to run with FactoryTalk Linx. You must have RSLinx Classic and FactoryTalk Linx installed to complete the conversion.
  • If the application includes alarm block tags, the conversion process creates direct references for each of the block tags imported. The direct reference is based on the original block tag name and address, with the modifier "L" appended. The "L" modifier is followed by the number of elements to be read. The number is arrived at by dividing the number of bits that is defined for the block tag by the number of bits in each address element (assumed to be a 16-bit word). For example, if the original block tag had 47 bits defined, using the address N7:0, it would be converted to a direct reference as N7:0,L3.
  • If the application files are created with an earlier version
    FactoryTalk View
    ,
    FactoryTalk View
    will create a copy of the application for the current version and will not alter the earlier version.
  • PanelView Plus 7 Standard
    application will be converted to
    PanelView Plus 7 Performance
    or custom size application, and the application limits will be removed. If you want a
    PanelView Plus 7 Standard
    application, specify the project window size in the
    Project Settings
    dialog box after the application is imported.
  • Compact Machine Edition application will be converted to a regular non-compact application, and the application limits will be removed. If you want a
    PanelView Plus 6 Compact
    application, specify the project window size in the
    Project Settings
    dialog box after the application is imported.
You can use the current version application files to create previous version runtime files in
FactoryTalk View Studio
.
For information about the features supported in different versions of
FactoryTalk View
, see "Appendix G" in
FactoryTalk View ME
User's Guide
.
You cannot import applications that were created with later versions of
FactoryTalk View Studio
than the one you are presently running. For example, if you are running Version 7.0, you cannot import an application that is created with Version 8.0.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal