Configure download drivers
Before you can transfer files between your desktop computer and a terminal on the network, you must configure a driver on each machine. The type of driver you need depends on the kind of network that connects the two.
To configure a download driver on your desktop computer
- InFactoryTalk View Studio, select theCommunicationstab of theExplorerwindow.
- Right-click the top level device that identifies your computer, and selectAdd Driver.
- Select the driver for the network type the terminal is on and clickOK.
- In the driver configuration window that opens, set up the driver and clickOK.
When you return to the
Communications Explorer
, the new driver will appear in the tree.To configure a download driver on the terminal
- Start the terminal and go to Configuration Mode.
- In thedialog box, clickFactoryTalk View ME StationTerminal Settings.
- SelectNetworks and Communications >.FactoryTalk LinxCommunications
- Select the network type the terminal is connected to, and then clickEdit Driver.
- In the driver configuration window that opens, set up the driver and clickClose. The driver must be for the same network type that you configured on the desktop computer.
- Restart the terminal to load the new configuration.
To communicate with the terminal
- InFactoryTalk View Studio, select theCommunications Explorer.
- Right-click the network icon below the top level device that identifies your computer, and selectStop Browsing.
- Right-click the same icon again and selectStart Browsing. The terminal you have just configured appears as a node under the driver, along with any other devices on the network that have this driver set up.
Provide Feedback