- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
Accordion
Expand or collapse content blocks when a user selects content blocks
Properties
Name | BrowseName | DataType | Description |
---|---|---|---|
Expanded | Expanded | Object status at runtime (True: the object is expanded, False: the object is compressed) | |
Height | Height | Height of the window. It can assume values greater than or equal to zero. The Auto value sets the height equal to the height of the content (in this case, in the absence of content the object collapses) | |
Style | Style | Graphic style applied to the control | |
Header | Header | Accordion header | |
Content | Content | Content of the accordion | |
Move target | MoveTarget | (Inherited from Container) | |
Visible | Visible | (Inherited from Element) | |
Enabled | Enabled | (Inherited from Element) | |
Opacity | Opacity | (Inherited from Element) | |
Left margin | LeftMargin | (Inherited from Element) | |
Top margin | TopMargin | (Inherited from Element) | |
Right margin | RightMargin | (Inherited from Element) | |
Bottom margin | BottomMargin | (Inherited from Element) | |
Width | Width | (Inherited from Element) | |
Horizontal alignment | HorizontalAlignment | (Inherited from Element) | |
Vertical alignment | VerticalAlignment | (Inherited from Element) | |
Rotation | Rotation | (Inherited from Element) |
Provide Feedback