Recipes editor customization

Instead of using the default recipes editor, you can design a custom recipes management interface.
TIP: You can develop a custom recipes management interface based on the objects reused from the default recipes editor. For more information, see Reuse objects from the default recipes editor.

Graphical objects and scripts for ingredients

IMPORTANT: While building your custom recipe management solution, you must include the objects from these NetLogic scripts.
Item
Functions
Usage
RecipesEditor
object
  • Contains other graphical objects that enable you to manage recipes.
  • Defines the reference recipe schema
In the
Properties
pane, in the
RecipeSchema
property, select a recipe schema.
RecipesEditorUISetup
NetLogic
Create the following set of objects for each ingredient of the selected recipe schema:
  • A
    Text box
    object with the name of the ingredient
  • The graphical object most suitable for changing the value of the ingredient, based on the ingredient data type (
    Text box
    ,
    Spin box
    ,
    Checkbox
    ,
    Date and time or Duration
    ).
    NOTE: At runtime, the value of this graphical object is copied automatically to the
    Edit model
    object.
To create the graphical objects, right-click
RecipesEditor
or
RecipesEditorUISetup
and select
Execute Setup
.

Stored recipes selection

Item
Functions
RecipesComboBox
object
  • Inserts the name of a recipe to store in the database associated with the recipe schema referenced in the
    RecipesEditor
    object
  • Displays the names of the recipes stored in the database
In
RecipesComboBox
,
RecipesEditorComboBoxLogic
NetLogic
  • Reads the data of the recipes stored in the database
  • Displays the recipes names in
    RecipesComboBox
    and displays the values of the ingredients

Recipes management

NOTE: The following button objects invoke the respective methods of the recipe schema object.
Item
Function
SaveButton
object
Save or update in the database the recipe written or selected in
RecipesComboBox
In
SaveButton
,
RecipesEditorSaveButtonLogic
NetLogic
DeleteRecipeButton
object
Delete the selected recipe from the database by using
RecipesComboBox
LoadButton
object
Load the selected recipe from the controller to the
FTOptixApplication
by using
RecipesComboBox
ApplyButton
object
Apply the selected recipe on the controller by using
RecipesComboBox

Notifications

Object
Function
OutputMessage
object
When the user saves, deletes, loads or applies a recipe, an output message displays for five seconds.
TIP: To change the message retention time, double-click the
RecipesEditorOutputMessageLogic
NetLogic script and change the value expressed in milliseconds.
RecipesEditorOutputMessageLogic
NetLogic
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal