Configure the authentication mode

Configure the authentication mode

Change the default authentication mode to allow local users and domain users to log on at runtime.
Prerequisites
To allow Active Directory users to authenticate, either:
  • Obtain the Active Directory domain name and server address.
  • Ensure that the
    Windows
    client is joined to the Active Directory domain.
To allow LDAP users to authenticate, obtain:
  • LDAP server address
  • CA certificate file
  1. To configure the authentication mode
  2. In
    Project view
    , select the root node.
  3. In
    Properties
    , expand
    Authentication
    , and then in
    Authentication mode
    , select the authentication type that allows specific users to log on:
    • Model only
      . Users created in
      FactoryTalk Optix Studio
      .
    • Local only
      . Local machine users.
    • Domain only
      . Active Directory and LDAP users.
    • Domain and local
      . Active Directory, LDAP, and local machine users.
    • Any
      . Users of any type.
  4. (optional) Set
    DefaultUserFolder
    to change the default folder to contain user objects.
    TIP: The default folder to contain user objects is
    Security
    Users
    . When a domain user logs in at runtime, a corresponding user object appears in the folder specified.
  5. (Domain only) In
    Default domain name
    , enter the default domain name for domain users that log on at runtime.
    TIP: If you leave Default domain name blank, the domain name is set based on the Active Directory domain joined by the
    Windows
    client or retrieved from the LDAP server.
  6. ( Doma in only) In
    Default server address
    , enter the Active Directory or LDAP server address.
    TIP: If you leave Default server address blank, the Active Directory server address is set based on the Active Directory domain joined by the
    Windows
    client.
    TIP: If you do not specify the port in the server address, the default 389 port is used.
  7. (LDAP only) In
    CA certificate file
    , select
    Browse
    and select the certificate file.
    TIP:
    To find items, start typing the item name to find in
    Select file
    .
    If the file does not appear in
    Select file
    , select
    Import file(s)
    and in
    Import file(s)
    , select the file to import and then choose
    Select
    .
    TIP: If you leave CA certificate file blank, the local
    Windows
    machine is used to authenticate the user. CA certificate file is required to authenticate against a specific LDAP server or use a Linux client.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal