Configure a button to close a dialog box
    To hide a dialog box at runtime, another object must call a specific method.
Prerequisites
Create a dialog box type. See Create a graphic object type.
- To configure a button to close a dialog box
 - Create a button object as a child of the dialog box type.For more information, see Create a graphic object from a type.
 - InEvents, next toMouseClick event, selectand select the
Closemethod. 
Provide Feedback