HSC instructions

Use high-speed counter (HSC) instructions to monitor and control the high-speed counter.
HSC instructions
Instruction
Description
HSC applies high presets, low presets, and output source values to the high-speed counter.
HSC_SET_STS manually sets or resets the HSC counting status.
HSCE starts, stops, and reads accumulator value.
HSCE_CFG is the high-speed counter configuration.
HSCE_CFG_PLS is the high-speed counter Programmable Limit Switch configuration.
HSCE_READ_STS reads high-speed counter status.
HSCE_SET_STS manually sets/resets high-speed counter status.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal