HSCE_CFG_PLS

The HSCE_CFG_PLS instruction is used for HSC configuration with Programmable Limit Switch (PLS). This function is an additional set of operating modes for the high-speed counter. When operating in these modes, the preset and output data values are updated using user-supplied data each time one of the presets is reached. These modes are programmed by providing a PLS file that contains the data sets to be used.
Languages supported: Function block diagram, ladder diagram, structured text.
This instruction applies to the
Micro820
L20E,
Micro850
L50E, and
Micro870
L70E controllers.
HSCE_CFG_PLS
HSCE_CFG_PLS
HSCE_CFG_PLS parameters
Parameter
Parameter Type
Data Type
Description
Execute
Input
BOOL
Rising edge initiates the HSC configuration (HSCE Enable should be equal to FALSE).
A falling edge will clear all the output value.
Channel
Input
HSCE_CHANNEL
The HSCE channel.
InitAccumulator
Input
LINT
Accumulator initial value.
OFSetting
Input
LINT
Counter overflow limit value.
UFSetting
Input
LINT
Counter underflow limit value.
PLS_Data
Input
PLS2
Configuration values for High Preset (LINT), Low Preset (LINT), High Preset Output (UDINT), and Low Preset Output (UDINT).
PLS_Size
Input
USINT
PLS data size, and the maximum value is 24 for a plug-in.
PLS_Offset
Input
USINT
Offset to start with in the PLS data array.
OutputMask
Input
UDINT
Output mask for PLS functionality.
Done
Output
BOOL
HSC configuration action (initiated by this instruction) succeeds.
Error
Output
BOOL
Indicates that an error occurred.
ErrorID
Output
UINT
When an error occurs, ErrorID contains the error codes.

HSCE_CGF_PLS examples

HSCE_CGF_PLS function block diagram example
HSCE_CGF_PLS function block diagram example
HSCE_CGF_PLS ladder diagram example
HSCE_CGF_PLS ladder diagram example
HSCE_CGF_PLS text structure example
HSCE_CGF_PLS text structure example
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal