HSCE error codes

The following table describes the status error codes for HSCE instructions.
HSCE error codes
Error Code
Error Description
Corrective Action
0
The instruction successfully completed operation.
N/A
1
Invalid HSC configuration files.
Contact the Rockwell Automation technical support representative. For contact information, see:
2
Invalid HSC module type.
Correct the module type. For example, select the module type as plug-in.
3
Invalid HSC Slot ID.
Correct the Slot ID in the Channel input of the function block.
4
Invalid HSC ID.
Correct the HSC ID. For example, set 0 for counter 0.
5
Invalid mode for the Channel.
Contact Rockwell Automation technical support representative.
6
Invalid PLS Size.
PLS size must be <= 24 and the size of the PLS data array must be >= PLS size.
7
Invalid PLS offset.
PLS offset + PLS size must be within the size of the PLS data array.
8
Invalid InitAccumulator value.
Correct the InitAccumulator value. Maybe it is over the boundary or out range of the LP or HP limit (LP <= InitACC <= HP).
9
Invalid LP.
Correct the LP value. It might be over the boundary.
10
Invalid OF.
Correct the OF value.
11
Invalid UF.
Correct the UF value.
12
Invalid HP.
Correct the HP value.
13
There is no configuration for HSCE.
Contact the Rockwell Automation technical support representative.
14
Invalid HSCE state.
Check the HSCE-related function block to confirm the state of this function block.
15
Invalid plug-in module
Check the plug-in module to confirm it is an HSC module.
16
HSCE is running.
When HSC is counting, no configuration or setting status is allowed. HSCE_CFG and HSCE_CFG_PLS are executed while HSCE is running.
17
Stop HSC plug-in failure.
Contact the Rockwell Automation technical support representative.
18
Update rate write failure.
Contact the Rockwell Automation technical support representative.
19
Write number of plus failure.
Contact the Rockwell Automation technical support representative.
20
Write Apply ACC failure.
Contact the Rockwell Automation technical support representative.
21
Write ACC failure.
Contact the Rockwell Automation technical support representative.
22
Write Apply failure.
Contact the Rockwell Automation technical support representative.
23
Write number of PLS failure.
Contact the Rockwell Automation technical support representative.
24
Write under flow failure.
Contact the Rockwell Automation technical support representative.
25
Write over flow failure.
Contact the Rockwell Automation technical support representative.
26
Write low preset failure.
Contact the Rockwell Automation technical support representative.
27
Write high preset failure.
Contact the Rockwell Automation technical support representative.
28
Write low preset out failure.
Contact the Rockwell Automation technical support representative.
29
Write high preset out failure.
Contact the Rockwell Automation technical support representative.
30
Write out mask failure.
Contact the Rockwell Automation technical support representative.
31
Write PLS low preset out failure.
Contact the Rockwell Automation technical support representative.
32
Write PLS high preset out failure.
Contact the Rockwell Automation technical support representative.
33
Write PLS low preset failure.
Contact the Rockwell Automation technical support representative.
34
Write PLS high preset out failure.
Contact the Rockwell Automation technical support representative.
35
Write PLS offset failure.
Contact the Rockwell Automation technical support representative.
36
Write PLS number failure.
Contact the Rockwell Automation technical support representative.
37
Read status failure.
Contact the Rockwell Automation technical support representative.
38
Read high preset failure.
Contact the Rockwell Automation technical support representative.
39
Read low preset failure.
Contact the Rockwell Automation technical support representative.
40
Read ACC failure.
Contact the Rockwell Automation technical support representative.
41
Read number of pulse width failure.
Contact the Rockwell Automation technical support representative.
42
Read pulse width failure.
Contact the Rockwell Automation technical support representative.
43
Read number of pulse failure.
Contact the Rockwell Automation technical support representative.
44
Read update rate failure.
Contact the Rockwell Automation technical support representative.
45
Write status failure.
Contact the Rockwell Automation technical support representative.
46
Read low preset out failure.
Contact the Rockwell Automation technical support representative.
47
Read high preset out failure.
Contact the Rockwell Automation technical support representative.
48
Read PLS number failure.
Contact the Rockwell Automation technical support representative.
49
N/A
Contact the Rockwell Automation technical support representative.
50
Write apply status failure.
Contact the Rockwell Automation technical support representative.
51
Invalid channel input.
Contact the Rockwell Automation technical support representative.
52
Read touch probe failure.
Contact the Rockwell Automation technical support representative.
53
Write reset ACC failure.
Contact the Rockwell Automation technical support representative.
54
Start HSC failure.
Contact the Rockwell Automation technical support representative.
55
Counter is disabled.
The HSC counter is disabled. Check the Channel configuration to verify if the HSC counter is enabled.
56
Invalid output mask value.
Check if the output mask is within the valid range. For plug-in HSC module, the range is 0–65535.
57
Invalid high preset output.
Check the if the HP output is within the valid range. For plug-in HSC module, the range is 0–65535.
58
Invalid low preset output.
Check if the LP output is within the valid range. For plug-in HSC module, the range is 0–65535.
59
Not a supported UPM revision.
Check the revision configuration for the HSC plug-in module.
60
Not an HSC module is added.
Check if the actual plug-in module is an HSC module.
61
HSCE plug-in module is not configured.
Contact the Rockwell Automation technical support representative.
62
A UPM plug-in Write error occurs while changing HSC plug-in Mode to Non-run.
Contact the Rockwell Automation technical support representative.
63
A UPM plug-in Write error occurs while changing HSC plug-in Mode to run mode.
Contact the Rockwell Automation technical support representative.
64
A UPM plug-in Read error occurs while reading Output Status.
Contact the Rockwell Automation technical support representative.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal