HSCE_CFG

The HSCE_CFG instruction is used to configure high-speed counter.
Languages supported: Function block diagram, ladder diagram, structured text.
This instruction applies to the
Micro820
L20E,
Micro850
L50E, and
Micro870
L70E controllers.
HSCE_CFG
HSCE_CFG
HSCE_CFG parameters
Parameter
Parameter Type
Data Type
Description
Execute
Input
BOOL
Rising edge initiates the HSC configuration (HSCE Enable should be equal to FALSE).
A falling edge will clear all the output value.
Channel
Input
HSCE_CHANNEL
The HSCE channel.
InitAccumulator
Input
LINT
Accumulator initial value.
OFSetting
Input
LINT
Counter overflow limit value.
UFSetting
Input
LINT
Counter underflow limit value.
HPSetting
Input
LINT
High Preset (HP) Value of HSCE.
LPSetting
Input
LINT
Low Preset (LP) Value of HSCE.
PLS_Offset
Input
USINT
Offset to start with in the PLS data array.
OutputMask
Input
UDINT
Output mask for Programmable Limit Switch (PLS) functionality.
HPOutput
Input
UDINT
High preset outputs state.
LPOutput
Input
UDINT
Low preset outputs state.
Done
Output
BOOL
HSC configuration action (initiated by this instruction) succeeds.
Error
Output
BOOL
Indicates that an error occurred.
ErrorID
Output
UINT
When an error occurs, ErrorID contains the HSCE error codes.

HSCE_CGF examples

HSCE_CGF function block diagram example
HSCE_CGF function block diagram example
HSCE_CGF ladder diagram example
HSCE_CGF ladder diagram example
HSCE_CGF structured text example
HSCE_CGF structured text example
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal