HSCE_READ_STS
The instruction is used to read current HSC status.
Languages supported: Function block diagram, ladder diagram, structured text.
This instruction applies to the
Micro820
L20E, Micro850
L50E, and Micro870
L70E controllers.HSCE_READ_STS

Parameter | Parameter Type | Data Type | Description |
|---|---|---|---|
Enable | Input | BOOL | If Enable is True then HSC2StsInfo is updated. |
Channel | Input | HSCE_CHANNEL | The HSCE channel. |
Valid | Output | BOOL | HSC2StsInfo is Valid if TRUE. |
HSCEStsInfo | Output | HSCE_STS | Counter overflow limit value. |
Error | Output | BOOL | Indicates that an error occurred. |
HSCE_READ_STS examples
HSCE_READ_STS function block diagram example

HSCE_READ_STS ladder diagram example

HSCE_READ_STS text structure example

Provide Feedback