Plug-in modules
The 2080 plug-in modules are attached to the
Micro800
controller to extend controller capability without increasing the controller's footprint. Use plug-ins for adding I/Os, communications, memory backup, and specialty capabilities.Micro820
L20E, Micro850
L50E, and Micro870
L70E controllers support plug-in modules. You can configure whether
to fault the controller when the plug-in module is absent.The following image shows a
Micro870
L70E controller configuration with
three plug-in modules. Use the PLUGIN_INFO instruction to verify whether a plug-in module is
present.Micro870 L70E controller configuration with three plug-ins

After attaching a plug-in module to the controller:
- InProject Organizer, the<plug-in-catalog-number>node is created under . To open the<plug-in-catalog-number>page, double-click the<plug-in-catalog-number>node.
- On the<plug-in-catalog-number>page, select a node to open the corresponding page and configure the plug-in settings.
Catalog Number | Type | Description |
|---|---|---|
2080-IF2 | Analog | 2-channel Voltage/Current Input |
2080-IF4 | Analog | 4-channel Voltage/Current Input |
2080-OF2 | Analog | 2-channel Voltage/Current Output |
2080-RTD2 | Analog | 2-channel Resistance Thermometer Detector |
2080-TC2 | Analog | 2-channel Thermocouple |
2080-DNET20 | Communication | DeviceNet |
2080-SERIALISOL | Communication | RS232/485 isolated serial port |
2080-IQ4 | Digital | 4-point digital input module |
2080-IQ4OB4 | Digital | 8-point digital combination module |
2080-IQ4OV4 | Digital | 8-point digital combination module |
2080-OB4 | Digital | 4-point digital output module |
2080-OV4 | Digital | 4-point digital output module |
2080-OW4I | Digital | 4-point relay output module |
2080-MEMBAK-RTC2 | Specialty | Memory backup and real-time clock (RTC) |
2080-SDMEMRTC-SC | Specialty | MicroSD card and high accuracy RTC It is not an Allen-Bradley® plug-in. It is from Rockwell Automation Encompass™ Product Partner-Spectrum Controls. |
2080-MOT-HSC | Specialty | Operates in high-speed counter mode or motion axis feedback mode |
2080-TRIMPOT6 | Specialty | 6-channel trimpot analog input |
Provide Feedback