Delete a plug-in module from the controller

Deleting a plug-in module removes the input and output variables from the controller configuration.
After deleting a plug-in module, update the Project Organization Units, interrupt definitions, Modbus address mappings, MicroLogix mappings, and DNP3 mappings that use the input and output variables of the plug-in module.
To delete a plug-in module from the controller
  1. In
    Project Organizer
    , go to
    I/O Configurations
    Plug-in
    .
  2. Under
    Plug-in
    , right-click the module, and then select
    Delete
    .
After deleting a plug-in module, the slot numbers of other plug-in modules remain unchanged.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal