Add a plug-in module to the controller

Use plug-ins to expand
Micro800
controllers for extra I/Os, communications, memory backup, and specialty capabilities.
To add a plug-in module to the controller
  1. In
    Project Organizer
    , go to
    I/O Configurations
    Plug-in
    .
  2. Right-click
    Plug-in
    , and then select
    New module
    .
  3. In
    Add module
    , select a plug-in module, and then select
    Add
    .
  4. In
    Devices definition
    , configure the slot, revision, and controller fault settings, and then select
    OK
    .
    TIP: To open the configuration page of a plug-in module, in
    Project Organizer
    , double-click
    <plug-in-ID>
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal