Independently released plug-in modules

Each release of
FactoryTalk Design Workbench
includes a set of plug-in modules for
Micro800
controllers, which can be added to the controller, and then configured using the
FactoryTalk Design Workbench
plug-in configuration workspace.
Some plug-in modules are released and available independently from the software release. They come with a support package that, when installed, updates the
FactoryTalk Design Workbench
software.
After you add an independently released plug-in module, the plug-in module is available in
Project Organizer
under the
Plug-in
node. Configuration of independently released plug-in modules follows the same procedure as other plug-in modules in
FactoryTalk Design Workbench
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal