Adjust the Workspace Pane
You cannot directly position the Workspace Pane, but you can move the Asset View. To maximize the area of the Workspace Pane, close, hide, or float the Asset View.
If multiple tabs are shown in the Workspace Pane, you can change the order in which the tabs are shown. Click the tab you want to move, and drag it to the desired position.
You can also show the tabs in separate vertical or horizontal panes. Right-click a tab and select:
- New Horizontal Tab Groupto put that tab in a separate horizontal pane.
- New Vertical Tab Groupto put that tab in a separate vertical pane.
- Move to Previous Tab Groupto move the selected tab to the previous pane (up or to the left depending on whether the screen is split horizontally or vertically).
- Move to Next Tab Groupto move the selected tab to the next pane (down or to the right depending on whether the screen is split horizontally or vertically).
Provide Feedback