Items in Options dialog box: Extended Properties
The following table describes the items in the
Options dialog box: Extended Properties
.Items | Descriptions |
|---|---|
Add | Adds an empty row to configure an extended property. |
Delete | Deletes a selected row of extended property. |
![]() | Selects all the extended property rows. |
![]() | Selects one extended property row. |
Property Name | Click in the empty cell of this column to enter an extended property name. This cell cannot be empty. If an extended property name is empty, you cannot save it or add another empty row. |
Property Value | Click in the empty cell of this column to enter en extended property value. This cell can be empty. |
Provide Feedback