Can't enter Design mode
This could happen for several reasons:
- You might not have the permissions to enter Design mode.
- Someone else may be in Design mode. Only one user at a time can be in Design mode. Examine the audit log to see if someone else is in Design mode and if so, who.
- If the server is not activated, you cannot enter Design mode (or view logs). To see if the server is activated, selectHelp > About. UnderComponentsselectFactoryTalk AssetCentre Server Features. Then in the left pane below that selectFactoryTalk AssetCentre Server. Activation information for the server is shown on the right. The word LICENSED indicates that it is activated.If the server needs to be activated, first clickRefreshin theAboutdialog box. If the server is still not activated, see your system administrator. The FactoryTalk Activation Manager help file may be useful in determining how to activate the server.
- The server, database, or FactoryTalk Directory may be offline or unavailable.
- If the Design mode button is unavailable, the above issues are not the cause, and showing theSchedules,Searches, andArchivetabs show a blank screen or the messagereading informationfor an inordinately long time, then reboot the client computer and theDesignbutton should become available.
Provide Feedback