View the Audit Log
The Audit Log shows database information regarding actions users perform in the system, such as making edits to a Logix 5000 project or checking out a file from the FactoryTalk AssetCentre database.
Prerequisites
- To view the Audit Log, you must be grantedView Audit Logpermission. If you do not have rights to view the log, the messageYou do not have permission to view the selected logwill appear.
To view the Audit Log
- SelectView > Logs, or click theLogsbutton.
- SelectView > Audit Log, or click theAudit Logbutton.
Provide Feedback