Create or modify a search schedule
You can add a schedule to or modify the scheduled settings of a previously saved search definition. You might want to do this if, for example, a search was scheduled to run once daily and now you want it to run at the end of every eight-hour shift. You can also add a schedule to a currently unscheduled search definition.
Prerequisites
- To modify a search, you must be granted theView a SearchandWritepermissions.
- To modify a scheduled search, you must also be granted theEdit a schedulepermission.
To create or modify a search schedule
- SelectView > Searches, or click theSearchesbutton.
- Select the search row for which you want to create or modify a schedule.
- SelectEdit > Properties, or click
.TIP:You can also click the gray button in theTiming Propertiescell of the search row. - Complete the(Search Name) Timing Propertiesdialog box.
- ClickOK.TIP:To designate a list of recipients or set the time zone for a search report, modify theScheduled Search Operationtab.
Provide Feedback