RA Drive operation properties for disaster recovery

Following are all possible settings for disaster recovery schedules for RA drive assets.
These settings are used for two purposes:
  • Specify default disaster recovery schedule settings for RA drives in
    Tools > Options
    .
  • Specify the settings of a particular RA drive asset in an existing schedule on the
    Schedules
    tab. Changes to the settings within a schedule override the default settings for that instance.
Unless noted otherwise, each setting applies to backup schedules and backup and compare schedules.
Event Settings
  • Master File Path Name
    (Only available when editing an existing schedule, not when setting defaults.) This field specifies the master file to be used in disaster recovery operations. Files are kept in archive where several versions of the same file may be stored. By default, disaster recovery operations use the pinned version of the specified file or, if no version has been pinned, the most recent version of the device's configuration data file. If you want to specify another version for the master file, click within this field and then click browse_button_small. Before you can edit this field, the device must have its configuration data defined in the device's properties.
  • (Backup and compare schedules only) Promote New Upload to Master
    This defaults to
    False
    . If set to
    True
    , when differences are detected this uploads the current file from the physical asset to archive and makes that version the master file for the asset.
  • (Backup and compare schedules only) Report Incremental Differences
    This option determines which differences are included in the backup and compare report. Set this option to
    True
    to only include those differences found since the last report was run. Set this option to
    False
    to include all differences found between the master file in the FactoryTalk AssetCentre Archive and the file in the device. To set this option to
    True
    , you must select
    Promote New Upload to Master
    (above).
(Backup and compare schedules only) Asset-specific properties
  • Compare All
    Select
    True
    to compare all data fields within a file. Select
    False
    to compare only editable fields within a file.
Email notification
To complete any of the following fields by selecting addresses from the FactoryTalk AssetCentre Address Book, click the field, and then click browse_button_small. Complete the
Contacts and Groups
dialog box.
An email message will be sent to only one of these lists. For example, if differences are found when a backup and compare schedule runs, an email is sent to those on the
Event Compare Differences Detected
list. No email is sent to those on the
Event Completed
list.
  • (Backup and compare schedules only) Event Compare Differences Detected
    The email addresses separated by semicolons (;) to which notification will be sent if the compare finds differences between the master file for the asset stored in the FactoryTalk AssetCentre Archive and the configuration of the physical asset.
  • Event Completed
    The email addresses separated by semicolons (;) to which notification will be sent when the operation completes for the asset. If a backup and compare schedule completes without differences, an email is sent to this list. If it completes with differences, an email is sent to the
    Event Compare Differences Detected
    list, not this list.
  • Event Failed
    The email addresses separated by semicolons (;) to which notification will be sent when the operation fails.
(Backup and compare schedules only) Attach report to email
  • Event Compare Differences Detected
    This defaults to
    False
    . Select
    True
    to attach a report of differences to the email if the backup and compare schedule finds variations between the asset's master file stored in the FactoryTalk AssetCentre Archive and the configuration of the physical asset.
  • Event Completed
    This defaults to
    False
    . Select
    True
    to attach a report to the email regarding whether or not the backup and compare event completed successfully.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal