Allen-Bradley PanelView operation properties for disaster recovery
Following are all possible settings for disaster recovery schedules for Allen-Bradley
PanelView assets.
These settings are used for two purposes:
- Specify default disaster recovery schedule settings for Allen-Bradley PanelView assets inTools > Options.
- Specify the settings of a particular Allen-Bradley PanelView asset in an existing schedule on theSchedulestab. Changes to the settings within a schedule override the default settings for that instance.
Unless noted otherwise, each setting applies to backup schedules and backup and compare schedules.
Event Settings
- Master File Path Name(Only available when editing an existing schedule, not when setting defaults.) This field specifies the master file to be used in disaster recovery operations. Files are kept in archive where several versions of the same file may be stored. By default, disaster recovery operations use the pinned version of the specified file or, if no version has been pinned, the most recent version of the device's configuration data file. If you want to specify another version for the master file, click within this field and then click
. Before you can edit this field, the device must have its configuration data
defined in the device's properties. - (Backup and compare schedules only) Promote New Upload to MasterThis defaults toFalse. If set toTrue, when differences are detected this uploads the current file from the physical asset to Archive and makes that version the master file for the asset.
- (Backup and compare schedules only) Report Incremental DifferencesNot available for Allen-Bradley PanelView devices.
Email notification
To complete any of the following fields by selecting addresses from the FactoryTalk AssetCentre Address Book, click the field, and then click
. Complete the
. Complete the Contacts and Groups
dialog box.An email message will be sent to only one of these lists. For example, if differences are found when a backup and compare schedule runs, an email is sent to those on the
Event Compare Differences Detected
list. No email is sent to those on the Event Completed
list.- (Backup and compare schedules only) Event Compare Differences DetectedThe email addresses separated by semicolons (;) to which notification will be sent if the compare finds differences between the master file for the asset stored in the FactoryTalk AssetCentre Archive and the configuration of the physical asset.
- Event CompletedThe email addresses separated by semicolons (;) to which notification will be sent when the operation completes for the asset. If a backup and compare schedule completes without differences, an email is sent to this list. If it completes with differences, an email is sent to theEvent Compare Differences Detectedlist, not this list.
- Event FailedThe email addresses separated by semicolons (;) to which notification will be sent when the operation fails.
(Backup and compare schedules only) Attach report to email
- Event Compare Differences DetectedThis defaults toFalse. SelectTrueto attach a report of differences to the email if the backup and compare schedule finds variations between the asset's master file stored in the FactoryTalk AssetCentre Archive and the configuration of the physical asset.
- Event CompletedThis defaults toFalse. SelectTrueto attach a report to the email regarding whether or not the backup and compare event completed successfully.
Provide Feedback