About Backup to Config Data wizard

How do I open Backup to Config Data wizard?
  1. In the asset tree, select a device that uses both Backup Data and Configuration Data binders, such as a Generic FTP Device or Siemens S7 Controller (STEP7).
  2. Select
    Tasks > Backup to config data
    . If
    Backup to config data
    is unavailable, make sure the selected device has a Backup Data binder and a Configuration Data binder set up in the device properties.
Use the the
Backup to Config Data
wizard to specify the version of a Backup Data binder to add as the most recent version of the Configuration Data binder.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal