Copy a version from Backup Data to Configuration Data
If the Backup Data becomes different than the Configuration Data, you may want to copy a backup version to the Configuration Data.
To copy a version of the Backup Data Binder to Configuration Data
- In the asset tree, select a device that uses Backup Data and Configuration Data binders, such as a Generic FTP Device or a Siemens S7 Controller (STEP7).
- SelectTasks > Backup to config data. If Backup to config data is unavailable, make sure the selected device has a Backup Data binder and a Configuration Data binder set up in the device properties.
- Use theBackup to Config Datawizard to select the version that you want to copy to Configuration Data.
Provide Feedback