Specify compare engines
Specify the compare engine (software program) to use for different types of files.
To specify compare engines
- SelectTools > Options.
- In the left column, clickCompare Engines.
- To add a new compare engine (or an existing compare engine with another configuration), click
. - Depending on if you are configuring the compare engine for Generic FTP or Remote Computer files, the configuration varies.
- To configure a compare engine for Generic FTP files or Remote Computer files:Select theEnable for DR Comparecheck box at the bottom of the dialog box. Fill in theDescription,Application,Parameters,Timeout (seconds), andReport Locationfields.
- To configure a compare engine for other file types:Keep theEnable for DR Comparecheck box at the bottom of the dialog box cleared. Fill in theDescription,Application,Parameters, andExtensionsfields.If you want this compare engine to be used when a compare is run on a file type that does not have a compare engine assigned to it, select theFallbackcheck box.
- To edit an existing compare engine configuration, select the compare engine configuration from the list and then edit the configuration as desired.
- ClickOK.
If two users edit a particular compare engine configuration simultaneously, the last (most recent) edit is kept. That is, the changes of the first user to click
OK
are not saved.Provide Feedback