Comparison Details dialog box

This dialog box shows details for an item selected in the
Comparison Overview
dialog box. When you close this dialog box, the
Comparison Overview
dialog box is shown and you can select another item to view details.
File
Includes options to save the detailed comparison results or to close the dialog box.
To save the results as a PDF file, select
Save detailed compare result as
.
Tree in left pane
Click on a node in the tree to see differences for that part of the program.
Path
Shows the path to the compared files on the local computer.
Object
Shows the location of the actual processor.
Chart
Shows the details of the comparison. Changes are indicated in red.
This component and color...
Means...
Absolute representation (address) all red (all digits in the address are red)
the absolute representation (address) was either deleted or inserted. This caused other addresses to shift.
Absolute representation (address) partially red (some but not all of the digits are red)
the Absolute representation (address) shifted to compensate for an inserted or removed address.
code all red
the code was added or removed when an address was added or removed.
code partially red
the code changed.
Absolute representation (address) or code all black
it did not change.
Disaster Recovery schedules have a very similar compare report for Siemens controllers.
In both Rockwell Automation Compare and Disaster Recovery compare operations, results shown in FactoryTalk AssetCentre show blank lines where an item was inserted or deleted in one of the comparison versions. In the report saved as a PDF file, however, blank lines are not shown.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal