View the Event Log
The Event Log shows database information regarding events that occur in the system. Events are generally system initiated, for example an upload occurred or a scheduled task completed.
Prerequisites
- To view the Event Log, you must be grantedView Event Logpermission. If you do not have rights to view the log, the messageYou do not have permission to view the selected logwill appear.
To view the Event Log
- SelectView > Logs, or click theLogsbutton.
- SelectView > Event Log, or click theEvent Logbutton.
Provide Feedback