View the Diagnostics and Health Log
The Diagnostics and Health Log provides information about the condition of automation devices. For example, a monitoring software product, such as RSNetWorxMD, detects a problem with a device on the automation network.
Prerequisites
- To view the Diagnostics and Health Log, you must be grantedView Diagnostics and Health Logpermission. If you do not have rights to view the log, a message will appear.
To view the Diagnostics and Health Log
- SelectView > Logs, or click theLogsbutton.
- SelectView > Diagnostics & Health Log, or click theDiagnostics & Health Logbutton.
Provide Feedback