Show file attachments and troubleshooting information

A record in any of the logs may contain a file attachment. If an attachment is generated for a log record, a paper clip icon newpaperclipicon appears in the leftmost column of the log record.
To view file attachment
  1. Select
    View > Logs
    , or click the
    Logs
    button.
  2. From the
    View
    menu, select the desired log, or click the button to show the
    Event Log
    ,
    Audit Log
    , or
    Diagnostics & Health Log
    .
    TIP:
    If Quick Search results are shown, you can also show file attachments and troubleshooting information for a record in the Quick Search results by clicking the
    Quick Search Results
    button.
  3. In the left-most column of the desired log record, double-click the paper clip icon newpaperclipicon, or with the record selected, in the
    Log Item Details
    pane at the bottom of the log, click newpaperclipiconfordetailspane.
  4. Complete the
    Attachments
    dialog box to view or save the file.
  5. Click
    Close
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal