About large file attachment
File attachments are generated automatically by the software product
that creates the log record, and may include information such as a comparison of ladder
files, or troubleshooting information such as a list of output errors.
File attachments have a 1 GB limit. Situations that could generate a
large file attachment include a disaster recovery schedule generating an exceptionally large
compare report or a scheduled search that returns a large amount of data.
Provide Feedback