Get started with FactoryTalk AssetCentre

This Quick Start series will guide you through the steps needed to begin using FactoryTalk AssetCentre. An overview of the process is provided below.
This Quick Start assumes that you have installed FactoryTalk AssetCentre
according to the instructions in the
FactoryTalk AssetCentre Installation Guide
.
Steps 1-4: Configure the system
System configuration is covered in the
FactoryTalk AssetCentre Installation Guide
, so this part of the process may be completed. To configure the system:
  • Step 1: Add users to the FactoryTalk Directory
  • Step 2: Add client computers to the system
  • Step 3: Configure security for FactoryTalk AssetCentre
  • Step 4: Add contacts to the FactoryTalk AssetCentre Address Book
Steps 5-7: Set up the asset tree
The asset tree is a representation of your plant including all the assets (anything from a device to a program to a procedure document) that you want to control, back up, or monitor. Everything that you do in FactoryTalk AssetCentre begins with an asset. To set up your asset tree:
  • Step 5: Design the asset tree
  • Step 6: Add assets
  • Step 7: Set security for the assets
Step 8: Set up Disaster Recovery schedules
FactoryTalk AssetCentre allows you to create schedules to run Disaster Recovery operations. The Disaster Recovery capability ensures quick and accurate file recovery by verifying your devices' program and configuration files against protected master files. The results (whether or not the operation completed successfully) can be sent to desired recipients by email. To set up Disaster Recovery schedules:
  • Step 8: Set up Disaster Recovery schedules
Conclusion and additional features
This Quick Start has provided the initial steps necessary to make use of your FactoryTalk AssetCentre system. Information on additional features can be found in this Help.
  • Conclusion and additional features
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal