FactoryTalk AssetCentre Security Configuration Export Tool
How do I open FactoryTalk AssetCentre Security Configuration Export Tool?
Open FactoryTalk AssetCentre Security Configuration Export Tool with one of the following methods:
- SelectStart > FactoryTalk AssetCentre Security Configuration Export Tool.
- Go to C:\Program Files (x86)\Rockwell Software\AssetCentre Server\Bin, and then openRockwellAutomation.FTAssetCentre.SecurityConfigurationExportTool.exe.TIP:
- TheRockwellAutomation.FTAssetCentre.SecurityConfigurationExportTool.exeis installed in C:\Program Files (x86)\Rockwell Software\AssetCentre Server\Bin by default.
- You can move this tool to the folder convenient to use. If so, the above methods are not available and you can open it directly.
FactoryTalk AssetCentre Security Configuration Export Tool can export the security configuration of assets in the asset tree as an XML file. The file is exported to %UserProfile%\Documents. We recommend that you use this tool as an administrator of
FactoryTalk AssetCentre
system.
TIP:
- If you have no privilege to use this tool, please contact the administrator to grant you theWritepermission for the computer and theReadpermission for theFactoryTalk AssetCentredatabase.
- We recommend that you open the XML file with Notepad.
Provide Feedback