Extended Properties dialog box

How do I open the Extended Properties dialog box?
  • While adding a device asset to the asset tree or editing an existing device asset's properties, under the
    Extended Properties
    category of the asset's properties dialog box, click the
    Properties Configuration
    box, and then click the browse button.
Customize extended properties to store extra information for an asset besides its default properties.
Use the
Extended Properties
dialog box to configure extended properties for a specific device asset, including:
  • Edit extended property name and value configured by the
    Options dialog box: Extended Properties
    .
  • Add or delete extended properties.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal