Controller I/O dialog box

How do I open the Controller I/O dialog box?
  • While adding an Allen-Bradley Logix 5000 Controller, Allen-Bradley MicroLogix Controller, Allen-Bradley PLC-5 Controller, or Allen-Bradley SLC 500 Controller asset to the asset tree or editing any of the assets' properties, under the
    Controller I/O
    category of the asset's properties dialog box, click the
    Controller I/O Listing
    box, and then click browse_button_small.
Use the
Controller I/O
dialog box to configure I/O modules for Allen-Bradley Logix 5000 Controller, Allen-Bradley MicroLogix Controller, Allen-Bradley PLC-5 Controller, and Allen-Bradley SLC 500 Controller assets. With this dialog box, you can:
  • Add or delete I/O modules.
  • (For Allen-Bradley Logix 5000 Controller only) Load I/O modules from the latest or pinned version of the configuration data file.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal