Items in the Controller I/O dialog box
The following table describes the items in the
Controller I/O
dialog box.Items | Descriptions |
|---|---|
Add I/O | Adds an empty row to configure an I/O module. |
Delete I/O | Deletes a selected row of an I/O module. |
Overwrite with Current ACD | This option is only available for Allen-Bradley Logix 5000 Controller device assets. Loads I/O modules from the latest or pinned version of the configuration data file. Any existing I/O modules will be replaced. To load I/O modules, make sure a configuration data file is configured for the device. |
Name | Shows the name of an I/O module. Each module name must be unique. |
Catalog Number | Shows the catalog number of an I/O module. The catalog number cannot be empty. |
Major Revision | Shows the major revision of an I/O module. |
Minor Revision | Shows the minor revision of an I/O module. |
Provide Feedback