Schneider Addressing dialog box
You can open the Schneider Addressing dialog box while adding a device to the asset tree or while editing a device's properties.
While adding an asset to the asset tree:
- If you are not already in Design mode, click
. - Drag a Schneider Controller (Control Expert) from the Asset Catalog to a container in the Asset View.
- Click anywhere within theAddressing Infofield and click
.
While editing an asset properties:
- If you are not already in Design mode, click
. - Double-click a Schneider Controller (Control Expert) in the tree.
- Click anywhere within theAddressing Infofield and click
.
Use the
Schneider Addressing
dialog box to provide the communication information necessary to connect to the Schneider Controller (Control Expert). Provide Feedback