Specify addressing information for FactoryTalk Optix Runtime (Embedded)
You must be connected to the control network to specify addressing information for the device.
To specify the addressing information
- Open asset properties, click anywhere in theAddressing Infofield, and then click
. Use the Selecting Device for Asset Typedialog box to browse the network for the FactoryTalk Optix Runtime (Embedded) that you want to add. When you have found the desired device, select it, and then clickSelect. - Complete the remaining fields as needed, and then selectOK.
Provide Feedback