Security Configuration dialog box

You can open the
Security Configuration
dialog box while adding a FactoryTalk Optix Runtime (Embedded) asset to the asset tree or editing a FactoryTalk Optix Runtime (Embedded) asset' s properties.
While adding an asset to the asset tree:
  1. If you are not in Design mode, click design_mode_button.
  2. Drag a FactoryTalk Optix Runtime (Embedded) asset from the asset catalog to add it to the asset view.
  3. Click anywhere within the
    Security Configuration
    field, and then click browse_button_small.
While editing an asset's properties:
  1. If you are not in Design mode, click design_mode_button.
  2. Double-click a FactoryTalk Optix Runtime (Embedded) asset in the asset tree.
  3. Click anywhere within the
    Security Configuration
    field, and then click browse_button_small.
Use the
Security Configuration
dialog box to configure the security attributes that are necessary to connect to the FactoryTalk Optix Runtime (Embedded) devices.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal