Add FactoryTalk Optix Runtime (Embedded) dialog box

  1. To enter the
    Design
    mode if you are not already in it, click design-mode-button.
  2. In the
    Asset Catalog
    , expand the
    SCADA, EOI and FactoryTalk Items
    node.
  3. Drag a FactoryTalk Optix Runtime (Embedded) asset onto the tree in the asset view.
Use the
Add FactoryTalk Optix Runtime (Embedded)
dialog box to add a FactoryTalk Optix Runtime (Embedded) asset to the asset tree. You can add a FactoryTalk Optix Runtime (Embedded) asset in the root or in a container.
This asset allows you to run a schedule that backs up FactoryTalk devices that have FactoryTalk Optix embedded, such as the Allen-Bradley OptixPanel, Allen-Bradley OptixEdge, or Allen-Bradley Embedded Edge Compute module. FactoryTalk Optix applications designed using
FactoryTalk® Optix Studio™
version 1.6.4 or later are supported. To ensure optimal performance and compatibility with FactoryTalk AssetCentre, we recommend always applying the latest available hotfixes for any version of FactoryTalk Optix Studio.
The device is added to the asset tree as soon as this dialog box opens. Clicking
Cancel
in this dialog box abandons any changes made to the device properties, but leaves the device in the tree.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal