Select File dialog box
How do I open the Select File dialog box?
- SelectView > Assets Lifecycle, or click theAssets Lifecyclebutton.
- Click theAsset Inventorytab.
- Click
.
Use the
Select File
dialog box to select an RAAI file and a version, the assets included in which will be shown on the Asset Inventory
tab of the Assets Lifecycle
tab.The tree view on the left of the dialog box shows the assets as in the asset tree. Once an RAAI file is selected, on the right of the dialog box, select a version of an RAAI file to open. The following options help you quickly select the version:
- Filter by labelSelect this option to filter the RAAI files by label. Use this option if a label was created for any particular versions.
- Filter by versionSelect this option to filter the RAAI files by version. Use this option to select a particular version from the list.
- Latest versionSelect this option to use the latest version of the RAAI file. This options is selected by default.
Provide Feedback