Refresh lifecycle status of asset inventory

Refresh the lifecycle information of asset inventory on the FactoryTalk AssetCentre client with the FactoryTalk AssetCentre server. This operation doesn't need an Internet connection.
To refresh lifecycle status of asset inventory
  1. Select
    View > Assets Lifecycle
    , or click the
    Assets Lifecycle
    button.
  2. Click the
    Asset Inventory
    tab.
  3. Click
    Refresh
    . A progress bar shows.
  4. After the progress, the lifecycle information is updated from the FactoryTalk AssetCentre database to the client and the lifecycle status is updated on the asset list.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal