Synchronize lifecycle status of asset inventory
Synchronize the lifecycle information of asset inventory in the FactoryTalk AssetCentre server with the Rockwell Automation lifecycle website. The lifecycle synchronization is recommended to run during server null time (time when no scheduled tasks or user interaction is taking place) if possible.
With the synchronization process being based on product ID or catalog number quantity, it can take some time to complete based on the total collected, and will require server resources during runtime.
Make sure you have an Internet connection for this operation.
To synchronize lifecycle status of asset inventory
- SelectView > Assets Lifecycle, or click theAssets Lifecyclebutton.
- Click theAsset Inventorytab.
- If you have used an asset inventory file before and don't want to use another version, skip to Step 7.If this is the first time to use an asset inventory file, theAsset Inventorytab is empty. You need to specify an RAAI file. On the right of theAsset Inventory Filebox, click
. - On the left of theSelect Filedialog, select an RAAI file in the asset tree view.
- On the right of theSelect Filedialog, select an RAAI file version.
- Filter by labelSelect this option to filter the RAAI files by label.
- Filter by versionSelect this option to filter the RAAI files by version.
- Latest versionSelect this option to use the latest version of the RAAI file.
- ClickOK.
- ClickSync. A progress bar shows.
- After the progress, the lifecycle information is updated to the FactoryTalk AssetCentre database and the lifecycle status is updated on the asset list.
Provide Feedback