Integrate an editor for a Siemens controller

When FactoryTalk AssetCentre was installed, editors for Siemens S5 Controllers and S7 Controllers (STEP7) were integrated with FactoryTalk AssetCentre. If you install a new editor, you need to integrate it with FactoryTalk AssetCentre. If you uninstall an editor you need to remove the integration.
To integrate a new editor
  1. In
    Control Panel
    , open
    Add or Remove Programs
    .
  2. Select
    FactoryTalk AssetCentre Client
    and click
    Change
    .
  3. Click
    Next
    on the first page of the installation wizard.
  4. Choose
    Modify
    , and then click
    Next
    .
  5. Use the
    Custom Setup
    page to add or remove integration for an editor.
  6. Click
    Next
    and proceed with the installation, following the instructions on the screen.
For more installation instructions, see the
FactoryTalk AssetCentre Installation Guide
. Select
Help > Installation Guide
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal